Page top

Primary Contents

Question

What cables are used to connect the CX-Simulator to an OMRON Programmable Terminal to operate the Programmable Terminal?

Answer



The Programmable Terminal's pin allocation is the same as a Programmable Controller's pin allocation, so use the same cable that is used to connect the computer to a Programmable Controller.

The following tables show the cables that can be used.

Cables for Touch Panels with a 9-pin Connector

IBM PC/AT or compatibleXW2Z-200S-V/500S-V
PC98 computer, 25-pinXW2Z-200S/500S
PC98 computer, Half-pitch 14-pinXW2Z-200S/500S + XW2Z-S001

Cables for Touch Panels with a 25-pin Connector

IBM PC/AT or compatibleXW2Z-200P-V/500P-V
PC98 computer, 25-pinXW2Z-200P/500P
PC98 computer, Half-pitch 14-pinXW2Z-200P/500P + XW2Z-S001

Recommended Products

NT20, NT31 / 31C-V3, NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V4 / -AL[][]D-V4

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Terminals FAQ