![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Can NS-series and NT-series Programmable Terminals be used together on one RS-232C port or one RS-422 port on a Programmable Controller?
Answer
Yes, it is possible if you use 1:N NT Links. It is done the same way as wiring or settings for NS-series or NT-series only.
However, 4-wire RS-422 must be used.
NS-series do not support RS-485 (two-wire). Also, when an RS-232C port on the Programmable Controllers is used, NT-AL001 RS-232C/RS-422 Link Adapter is necessary.
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.