Page top

Primary Contents

Question

What is the difference in the way that serial ports A and B are used on NT31/631 Programmable Terminals?

Answer



1.Either serial port A or serial port B may be used to connect to the host. Both ports cannot be simultaneously connected to a host.

2.Screen data transfer can be done only using serial port A. Serial port B cannot be used for screen data transfer.

3.For details, refer to NT31/NT31C Setup Manual or NT631/NT631C Setup Manual.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Terminals FAQ