![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
The lamp does not light up even when Illuminating Type Push Button Switches are pushed.
Answer
Check the following points.
1. Is the polarity of the lamp is connected correctly?
2. Are the lamp's voltage specifications compatible with the applied voltage?
3. Terminals of the LED and the switch are separated and so it is necessary to connect them.
The terminal layout of the A16 is as follows.