Page top

Lead Contents

FAQ00414 of Proximity Sensors FAQ

FAQ No. FAQ00414

Primary Contents


What Proximity Sensors are available for applications that require heat resistance?


E2C-H Series of Heat-resistant Proximity Sensors is available. Normal Proximity Sensors have an ambient operating temperature range of -25 to 70°C. E2C-H Series has an ambient operating temperature range of -10 to 200°C.

E2C-H Series has the following characteristics:

Internal electronic components are placed in the amplifier section so that they are not subjected to high temperatures.

Heat-resistant parts are used for the case, solder, coil, cable and other components of the head section used in high temperatures.

These Sensors, however, are not filled internally with resin, and so the degree of protection is reduced.