Page top

Primary Contents

Question

Is it possible to display only "+" and "-"?

Answer



Yes, it is.

Models with binary-coded decimal (06 models) are available that display "+, -, +, -. . ." rather than "0, 1, 2, 3, 4, 5 . . . 9".

The models are the A7[]-206-PM and A7[]-206-PM-1.

Example:

Thumbwheel Switch
A7BS-206-PM

Output Code:

The signal between output terminal 1 and the COM terminal of the Thumbwheel Switch is used as the binary code.

Example of A7BS-206-PM

ModelSwitch Unit or
Connector
Common terminal
number
Terminals connected to
common
A7BSSwitch UnitC1248
Connector24567
Dial+ (0)
- (1)
+ (2)
- (3)
+ (4)
- (5)
+ (6)
- (7)
+ (8)
- (9)

Note:

1.The solid dot ● indicates that the internal switch is ON.

2.Numbers enclosed in parentheses are the dial displays for the A7BS-206.

Recommended Products

Z

Best-selling Basic Switch Boasting High Precision and Wide Variety

WL / WLM

Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

D4A-[]N

The Limit Switch with Better Seal, Shock Resistance, and Strength

Other Thumbwheel Switches FAQ