Page top

Lead Contents

FAQ03428 of Vision Sensors / Machine Vision Systems FAQ

FAQ No. FAQ03428

Primary Contents


Can the camera cable for the F500 Vision Sensor be extended?


The digital camera cable can be extended up to 10 m.

The standard length of a F500-VS Cable is 2 m, but 5-m and 10-m cables are also available.

To place an order, specify the desired length after the model number. (e.g., F500-VS 5M or F500-VS 10M)

The F500-VS Camera Cable includes the F500-VSD Camera Link Cable and the F500-VSP Camera Power Cable as a set.