Page top

Lead Contents

FAQ03432 of Vision Sensors / Machine Vision Systems FAQ

FAQ No. FAQ03432

Primary Contents


Console cables for Vision Sensors can be extended?


Standard cable length of the Console "F150-KP" is 2m. Other than this, however, cables of 5m and 10m length are also available.
When ordering, specify the cable length with the model name: F150-KP 5M or F150-KP 10M.
Console "F160-KP" is only available in length of 2m. This is because the console incorporates the IC which can not operate when voltage drop occurs due to the cable extension.
Therefore, it is recommended that the F160-KP should be used with standard length.