Page top

Lead Contents

FAQ01511 of Axial Fans FAQ

FAQ No. FAQ01511

Primary Contents

Question

What are the meanings of inlet and outlet?

Answer



1. Axial Fans

As shown in the following diagram, the side with the label attached is the outlet, and the opposite side is the inlet. The Fan can be installed with either side facing forward, but there is a greater chance of dust entering the Fan when the inlet side faces forward, which may necessitate a filter or other dust-preventive measure.

2. Box Fans

The inlet and outlet sides of Box Fans are specified for each model.

3. Examples of Inlet-and Outlet-side Fan Installation

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Axial Fans FAQ