Page top

Lead Contents

FAQ01519 of Axial Fans FAQ

FAQ No. FAQ01519

Primary Contents

Question

What precautions are necessary for installing products?

Answer



If users are likely to touch fan blades, be sure to install a finger guard.

Install a guard fence/net or the optional finger guard onto an area where an Axial Fan is installed.

Do not use a box fan without a finger guard. Otherwise, contact to the fan blade may cause injury.

Finger guards are available as the Optional Accessory "R87F-FG" which is selectable according to the size of an Axial Fan to be used.

Be sure to turn off power and confirm that fan blades stop moving before checking the operation or changing filters. Otherwise, contact to the fan blade may cause injury.

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Axial Fans FAQ