Page top

Lead Contents

FAQ01548 of Axial Fans FAQ

FAQ No. FAQ01548

Primary Contents

Question

Are there any specific application methods that will extend the life of an Axial-flow Fan?

Answer



Yes, the following methods will help extend the lifetime.

1.Keep the ambient temperature (i.e., temperature of the Fan itself) as low as possible.

→ Use the Fan at the inlet.

2.Do not subject the Fan to shock. (The bearing is especially susceptible to damage from shock and has a major effect on the Fan life.)

3.As much as possible, do not expose the Fan directly to dust and other airborne particles.

→ Install a filter.

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Axial Fans FAQ