Page top

Lead Contents

FAQ01607 of Axial Fans FAQ

FAQ No. FAQ01607

Primary Contents

Question

What is the maximum flowrate?

Answer



This is the flowrate of the Fan when the static pressure is set to 0 Pa with a flowrate meter. In other words, it is the flowrate when the Fan is operating in a hypothetical state completely free of resistance.

Unit: Qmax (m3⁄min)

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Axial Fans FAQ