Page top

Lead Contents

FAQ01617 of Axial Fans FAQ

FAQ No. FAQ01617

Primary Contents

Question

What is static pressure?

Answer



The pressure difference across the front to the back of the Fan generated by the discharged air, which is unaffected by air flow speed.

Unit: Ps (Pa)

1.The air pressure across the front to the back of the Fan does not change when the Fan is stopped.

2.Static pressure (Ps) is generated at the front of the Fan when it rotates.

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Axial Fans FAQ