Page top

Lead Contents

FAQ01622 of Axial Fans FAQ

FAQ No. FAQ01622

Primary Contents

Question

What is the maximum static pressure?

Answer



The pressure difference inside and outside the Unit when the flow rate is adjusted to zero (0 m3/min.) at the flow measurement unit. This would be the pressure in front of the Unit when the front of the fan was completely sealed.

Unit: Ps max. (Pa)

Recommended Products

S8VS

Multi-Function Indication Monitor for Production Site Visualization * (* Models with indication monitor)

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Axial Fans FAQ