![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is redundancy?
Answer
Redundancy is duplication. The probability of hazards arising from one malfunction in an electrical circuit can be minimized by creating partial or complete Redundancy (duplication).
The following diagram shows an example circuit where the use of two or more relays or switches in parallel enables performing the total function if one of them is malfunctioning.
Redundant Circuit Configuration Example Using Two Relays
Redundant Circuit Configuration Example Using Two Switches
Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards
The updated F3SJ is even easier to use.
Operator Presence Detection in Work Areas with Complex Shapes.