Page top

Primary Contents

Question

What is a positive common input?

Answer



It is an input mode where there are two inputs and both of them are connected to the positive side of the power supply. Both inputs will be at the same voltage, so if there is a short circuit between two terminals, it will not be detected.

If there is the possibility of a short circuit at the input, do not use this input method because it cannot detect faults, and it cannot ensure safe operation.

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Safety Relays FAQ