Page top

Primary Contents

Question

Why cannot Programmable Controller (PLC) or Programmable Terminal (PT) be used for safety circuits?

Answer



Industrial standards IEC60204-1(JIS B 9960-1) prescribes that the safety circuit should not be configured only with the Programmable Controller.

This comes from the general requirements of the IEC60204-1(JIS B 9960-1) that safety-related functions should be configured with the verified circuit technologies and components.

However, since circuits depending on the movement of programmable electronic devices may sometimes not fulfill these requirements, for this reason, Programmable Controller or Programmable Terminal cannot be used for safety circuits.

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Safety Relays FAQ