Page top

Primary Contents

Question

How does a forcibly guided contact work?

Answer



If an NO contact becomes welded, all NC contacts will maintain a minimum distance of 0.5 mm when the coil is not energized. Likewise if an NC contact becomes welded, all NO contacts will maintain a minimum distance of 0.5 mm when the coil is energized.
Refer to the following diagram.

The forcibly guided contact mechanism is a requirement of EN 50205 for Safety Relays.
Class A Safety Relays (i.e., all contacts are forcibly guided contacts) have the mark(*) on the nameplate.

Forcibly Guided Contact Mechanism (G7SA Safety Relays)

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Safety Relays FAQ