Page top

Lead Contents

FAQ03403 of RFID Systems FAQ

FAQ No. FAQ03403

Primary Contents


Are there any RFID antennas available which are compatible with movable cables (robot cables)?


Yes. The V600-H11-R for the Electromagnetic Coupling RFID System "V600 Series" is compatible with a movable cable, which is 50 cm in length.

Additionally, other antennas for the V600 Series such as Built-in Amplifier Type "V600-H07, -H11, -H51,-H52" and Amplifier part of the Separate Amplifier Type "V600-HA51" can be connected with the following robotic extension cables.

V600-A56 (Cable lengths = 3m)

V600-A55 (Cable lengths =5m)

V600-A50 (Cable lengths =10m)

V600-A51 (Cable lengths =20m)

V600-A52 (Cable lengths =30m)

Recommended Products


Introducing the Flagship CJ2 CPU Units, with Built-in Multifunctional Ethernet Port.


Cost-effective CP1E with Enhanced Expandability for Analog and Temperature Control


Motion, Logic, Safety, Vision and HMI in one

Other RFID Systems FAQ