![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How do I interpret the catalog values for mutual interference with Proximity Sensors?
Answer
Refer to the following figures.
Mutual Interference
Use Sensors with the values in the following table or higher when they are mounted facing each other or in parallel.
| Model | Item | M8 | M12 | M18 | M30 | |
| DC 2-Wire Models E2E-X[]D[] AC/DC 2-Wire Models E2E-X[]T1 | Shielded | A | 20 | 30 (20) | 50 (30) | 100 (50) |
| B | 15 | 20 (12) | 35 (18) | 70 (35) | ||
| Unshielded | A | 80 | 120 (60) | 200 (100) | 300 (100) | |
| B | 60 | 100 (50) | 110 (60) | 200 (100) | ||
Note:Values in parentheses apply to Sensors operating at different frequencies.
The values listed above are given in the precautions section of the catalog. Dimensions A and B are specified by the way in which the Proximity Sensors are arranged. If a gap cannot be provided between the Proximity Sensors, they can be used close together up to the catalog values in parentheses by using a standard model in combination with a model that has a different frequency.
Note:Two of the Sensors with a different frequency cannot be used near each other. Leave a gap of at least the value not in parentheses.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.