Page top

Primary Contents

Question

What are measures and malfunction mode when the relay of not being possible to connect it with the Proximity Sensor is connected?

Answer



Malfunction mode

1. The relay is not ON

When the proximity sensor does not meet the ON condition of the relay

2. The relay is not OFF

When the proximity sensor does not meet the OFF condition of the relay

3. The relay throbs

When the proximity sensor nearly meets the ON/OFF condition of the relay

Measures against malfunction

1. The relay is not ON

There are no measures.

2. The relay is not OFF or The relay throbs

Please put the bleeder resistance in parallel with the load. (Refer to the figure below.)

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Proximity Sensors FAQ