![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Will there be any problem if GLS Proximity Sensors are installed with the direction of the magnet section changed?
Answer
As shown in the following figures, there is no problem if the magnet section (GLS-M1) is rotated 180°. However, install it so that the direction of travel is in the direction of the arrow.
The sensing distance will decrease if the magnet section is mounted on a steel plate or other magnetic object. Check the sensing distance before operating GLS.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.