Page top

Primary Contents

Question

Please teach the principle of operation of capacitive proximity sensor the E2K type.

Answer



The circuit composition and the principle of operation are as follows.

1. Circuit composition

2. Principle of operation

When the metal or the dielectric approaches the electrode, the capacitance between a main electrode and ground potential increases by the effect of the electrostatic induction.

The CR oscillation circuit that starts oscillation depending on the capacitance change of this electrode is composed, and the approach of the sensing object is detected by increase of the oscillation amplitude.

When the sensing object is the dielectric, the change in the capacitance between a main electrode and ground potential grows by the relative permittivity large and it is easy for the sensor to detect it.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Proximity Sensors FAQ