Page top

Primary Contents

Question

What Proximity Sensors are available for applications that require heat resistance?

Answer



E2C-H Series of Heat-resistant Proximity Sensors is available. Normal Proximity Sensors have an ambient operating temperature range of -25 to 70°C. E2C-H Series has an ambient operating temperature range of -10 to 200°C.

E2C-H Series has the following characteristics:

Internal electronic components are placed in the amplifier section so that they are not subjected to high temperatures.

Heat-resistant parts are used for the case, solder, coil, cable and other components of the head section used in high temperatures.

These Sensors, however, are not filled internally with resin, and so the degree of protection is reduced.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Proximity Sensors FAQ