Page top

Primary Contents

Question

How is the UL standard of the sensor of the DC power system treated?

Answer



It is not necessary to use the UL standard certificated models in this case.
Please use the power supply certificated to the class 2 complying with the UL1310.

When you need to use the UL standard certificated sensors of the DC power system, Omron can provide the sensors that is certificated with the UL standards under the condition of "using in class 2 circuits".

Omron can provide the sensors with the UL standards certificated name-plate that is shown under the conditions of using in class 2 circuit.

Top of page
Site Information

OMRON Corporation Terms of Use Privacy Policy
c Copyright OMRON Corporation 2007. All Rights Reserved.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Proximity Sensors FAQ