Page top

Primary Contents

Question

Why is there a difference in the effect of surrounding metal between Shielded Proximity Sensors and Unshielded Proximity Sensors?

Answer



As shown in Figure 1, the surface of the detection coil on Shielded Proximity Sensors is covered with metal, so the flux is concentrated at the front of Sensors, which reduces the influence of surrounding metal.

As shown in Figure 2, the surface of the sensing coil on Unshielded Proximity Sensors is not covered with metal, so flux is also generated from the surface, which makes Sensors easily influenced by surrounding metal.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Proximity Sensors FAQ