Page top

Primary Contents

Question

What is the difference between EE-1010 and EE-1010-R Connectors with Cables?

Answer



EE-1010 uses a regular cable, but EE-1010-R uses a robot cable, which provides superior flexibility. (The robot cable can be bent more than approximately three times as many times as the regular cable. Use a bending radius of at least three times the diameter of the cable.)

Using EE-1010-R is recommended if the cable is to be connected to a moving part.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Photomicro Sensors FAQ