Page top

Primary Contents

Question

Can the EE-SX671 Photomicro Sensor be used in a magnetic field?

Answer



Yes, it is fundamentally possible to use EE-SX671 in a DC magnetic field, but operation must be confirmed by testing if the magnetic field is strong (on the level of affecting electronic circuits) or if EE-SX671 is used near the source of a high-frequency magnetic field.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Photomicro Sensors FAQ