![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Can regular lead wire be added in the middle of E69-DF[] Extension Cables when it is connected to E6[][] Absolute Encoders and H8P[] Cam Positionesr?
Answer
Trouble will occur in the sense that the rated specifications will not be met. To reduce the effects of noise, use a special E69-DF[] Extension Cable. Do not relay the cable using a terminal block. Doing so will cause the signal to be easily affected by other signal lines.
Applicable model combinations:
E6CP-AG5C-C/H8PS
E6C3-AG5C-C/H8PS
E6F-AG5C-C/H8PS
E6F-AB3C-C/H8PR
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.