![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Can the origin (phase "Z") be positioned with only the Rotary Encoder (without seeing ON/OFF of the output)?
Answer
1. In the E6B2-C and E6C2-CWZ[][], positioning the origin is almost possible by setting phase "Z" origin to cut face "D". (within ±20°)
E6B2-C
E6C2-CWZ[][]
2. In the E6C3-CWZ[][]H, positioning the origin is almost possible by making cut face "D" of the shaft and the direction of drawing out of the cable as the following figure. (within ±15°)
E6C3-CWZ[][]H
3. Please confirm ON point of phase "Z" output on the controller side and adjust the origin so cut face "D" and phase "Z" origin of other models are not suitable.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.