![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the method of confirming abnormalities of the number of output pulse (omission of the number of pulse) in the incremental rotary encoder?
Answer
It is possible to judge it by counting the number of pulse signals from phase Z signal to the next phase Z signal if there is phase Z output.
Moreover, it is possible to judge it by counting the number of pulse signals when the axis is made one rotation after a standard position somewhere is made to be understood in the axis and the chassis if there is no phase Z output.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.