Page top

Primary Contents

Question

What is the difference between incremental Rotary Encoder and absolute Rotary Encoder?

Answer



Incremental rotary encoder outputs the pulse corresponding to the rotation angle only while rotating, and is the counting measurement method that adds up the pulse from the measurement beginning point.

Absolute rotary encoder outputs the signal of position corresponding to the rotation angle by code. The Absolute position from the starting point is measured by the output code data. The position is memorized though the power supply is cut off.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Rotary Encoders FAQ