![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country.
Please contact OMRON Europe B.V. in Netherlands.
Question
How far should the shaft be inserted into the coupling?
Answer
The hollow section (corniced part) near the center of the coupling absorbs vibration and prevents Rotary Encoders becoming damaged due to vibration. To protect Rotary Encoders from vibration, insert the shaft into the coupling at least to the length given in the following table.
| Coupling model | Insertion |
| E69-C04B | 5.2 mm |
| E69-C06B | 5.5 mm |
| E69-C08B | 6.8 mm |
| E69-C10B | 7.1 mm |
| E69-C68B | 6.8 mm |
| E69-C610B | 7.1 mm |
| E69-C06M | 8.5 mm |
| E69-C10M | 10.5 mm |