Page top

Lead Contents

FAQ00541 of Temperature Controllers FAQ

FAQ No. FAQ00541

Primary Contents

Question

When can the manual reset be used for E5[]N/E5[]K Temperature Controllers?

Answer



The manual reset can be used for P or PD control. There is an offset for the set point when using P or PD control because there is no integral control action.
There is no offset if auto-tuning (AT) or self-tuning (ST) is used. The manual reset can be used to set the close to zero.
If the control output is high when the PV equals the SV, lower the control output for the manual reset.

Set the parameter in Level 1 Mode for the E5[]K, and in Adjustment Level for the E5[]N.

Applicable models: E5AK, E5EK, E5CK, E5AN, E5EN, E5CN, and E5GN

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Temperature Controllers FAQ