Page top

Lead Contents

FAQ00582 of Temperature Controllers FAQ

FAQ No. FAQ00582

Primary Contents


What is "Hunting" and "Overshooting"?


ON/OFF control action often involves the waveform shown in the following diagram. A temperature rise that exceeds the set point after temperature control starts is called overshooting. Temperature oscillation near the set point is called hunting. Improved temperature control is to be expected if the degree of overshooting and hunting are low.

Hunting and Overshooting in ON/OFF Control Action

Recommended Products


A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals


A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.


Easy to Use and Easy to Read.

Other Temperature Controllers FAQ