Page top

Lead Contents

FAQ01847 of Power Controllers FAQ

FAQ No. FAQ01847

Primary Contents


Can three G3PX Power Controllers for single-phase applications be combined for control of three-phase loads?


Three-phase loads are controlled by each having a phase angle separated by 120°, so three G3PX Units for single-phase applications cannot be used. Always use a Three-phase Controller to control three-phase loads.

Sometimes the G3PX-260E[] can be used for an open delta configuration (see the connection diagram below).

Note:The G3PX-220E[]/240E[] (20 A/40 A) cannot be used.

Recommended Products


New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays


Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other Power Controllers FAQ