Page top

Lead Contents

FAQ01851 of Power Controllers FAQ

FAQ No. FAQ01851

Primary Contents

Question

Which terminals should the G3PX Power Controller inputs be connected to?

Answer



It depends on the type of input.

1. Analog Inputs

(1) 4 to 20-mA or 1 to 5-V Inputs


Terminals: 4 and 5

Note:The terminals are the same (4 and 5) for both current and voltage inputs.

Input impedance: 250 Ω

(2) Analog Inputs Using External Main Setting

2. ON/OFF Pulse Inputs

Terminal numbers 3 to 5

(1) Power ON/OFF Pulse Signal Inputs

Example

(2) Contact ON/OFF Pulse Signal Inputs

Note:There is only one input of whatever kind. The G3PX may be damaged if there is more than one signal is input.

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other Power Controllers FAQ