Page top

Lead Contents

FAQ01940 of Power Controllers FAQ

FAQ No. FAQ01940

Primary Contents


If 200V is applied to the AC100V terminal, what will happen?


When the G3PX turns ON and a load current flows, a residual voltage is produced on the switching element.

The heating value will be obtained from the following formula.


Case of the G3PX-220EUN (with rated currents of 20A)
VRMS (residual voltage)=1.6V (output ON voltage drop in the brochure)
If the power consumption is indicated as P:
This is the power consumption of the G3PX.

In terms of calorie 1cal/s equals 4.19W, therefore:
32W÷4.19 ≒ approx.7.6cal/s

The residual voltage means the voltage lost inside the semiconductor when it turns ON.

Recommended Products


New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays


Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other Power Controllers FAQ