Question
What is the gradient setting?
Answer
The gradient setting is a function for adjusting the output variation using internal or external variable resistors, as shown in the following diagram. The gradient setting function is separate from the temperature control signals and is used to refine the output amount.
If the internal and external variable resistor controls are used at the same time, the internal variable resistor setting will take precedence.
Example:
If the internal gradient setting is 0%, the external gradient setting can be adjusted only between 0% and 80%.
Best-selling, general-purpose relays that can be selected based on operating environment and application
Power-switching Compact General-purpose Relays
Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.