Question
Why does the constant-current model sometimes have all indicators ON?
Answer
A constant-current model will sometimes not be able to perform control if used with a current load much smaller than the rated current.
Possible Countermeasures:
1. Adjust the CUR LIM adjuster until one of the level indicators turns OFF.
2. If using 50% or less of the rated current, increase the number of turns of the wire on the CT.
Example:
50% of the rated current: 2 turns
25% of the rated current: 4 turns
Applicable models: G3PX-2[][]EC/G3PX-2[][]DC Power Controllers
Best-selling, general-purpose relays that can be selected based on operating environment and application
Power-switching Compact General-purpose Relays
Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.