Page top

Lead Contents

FAQ01992 of Power Controllers FAQ

FAQ No. FAQ01992

Primary Contents


What is the minimum load current value that can be set?


The load current is limited to 1A at 100% output.

TRIAC or Thyristor output elements have a minimum holding current. If the load current is less than 1A, decrease in output signals cannot make output elements keep in the ON state, so that oscillating waveform may occur or they may not be turned ON.

Recommended Products


New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays


Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other Power Controllers FAQ