Page top

Lead Contents

FAQ01994 of Power Controllers FAQ

FAQ No. FAQ01994

Primary Contents

Question

How much heating value flows from the Electrical Regulator "G3PX"?

Answer



When the G3PX turns ON and a load current flows, a residual voltage is produced on the switching element.

The heating value will be obtained from the following formula.

Example:

Case of the G3PX-220EUN (with rated currents of 20A)
VRMS (residual voltage)=1.6V (output ON voltage drop in the brochure)

If the power consumption is indicated as P:
P=20A×1.6V
P=32W
This is the power consumption of the G3PX.

In terms of calorie 1cal/s equals 4.19W, therefore:
32W÷4.19≒approx.7.6cal/s

The residual voltage means the voltage lost inside the semiconductor when it turns ON.

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other Power Controllers FAQ