Page top

Lead Contents

FAQ02022 of Power Controllers FAQ

FAQ No. FAQ02022

Primary Contents

Question

What is phase control?

Answer




Phase control is control method in which the output amount is changed each half cycle. It enables high-precision temperature control.

Analog control of the output power is possible by receiving a 4 to 20-mA current output signal from the Temperature Controller.

The high-precision control makes the Temperature Controller resistant to external interference and the small heat shock means the heater life can be extended.

Note: Noise is generated, however, because it is not a zero-cross circuit.

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other Power Controllers FAQ