![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Can the V500-R521 Bar Code Readers laser be blocked with transparent acrylic boards or PET boards?
Answer
The V500-R521 uses a class 2 laser. It is thought that the power of the laser deteriorates from the reflection and refraction when passing through acrylic (transparent) or PET material. If the acrylic material is colored, the coloring also affects the power of the laser.
To completely block the laser beam, a laser light curtain can be used.
The specified wavelength of the V500-R521 is 650 nm.
Helium-Neon (He-Ne) ← Blue
OD2 ← Blocking level (OD2 is sufficient for a class 2 laser.)
Use a light curtain as mentioned above by gluing it to the acrylic or PET material.
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.