Page top

Primary Contents

Question

Are there any RFID antennas available which are compatible with movable cables (robot cables)?

Answer



Yes. The V600-H11-R for the Electromagnetic Coupling RFID System "V600 Series" is compatible with a movable cable, which is 50 cm in length.

Additionally, other antennas for the V600 Series such as Built-in Amplifier Type "V600-H07, -H11, -H51,-H52" and Amplifier part of the Separate Amplifier Type "V600-HA51" can be connected with the following robotic extension cables.

V600-A56 (Cable lengths = 3m)

V600-A55 (Cable lengths =5m)

V600-A50 (Cable lengths =10m)

V600-A51 (Cable lengths =20m)

V600-A52 (Cable lengths =30m)

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other RFID Systems FAQ