![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What happens when multiple Sensors are used and they interfere with each other? What can be done to resolve the problem?
Answer
Mutual interference:
An error occurs in the analog value to the Analog Input Unit of the Digital Panel Indicators or Programmable Controllers.
(For example when the input is 10 mA, an input of 4 mA is indicated.)
When this happens, the error indicator (red LED) will begin to flash.
Countermeasure:
Place the Sensors apart from one another so that they do not interfere with each other.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.