![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
If coating compositions and/or water drops adhere to the surface of Ultrasonic Sensors, is the operation affected?
Answer
Yes, it is.
Since the sensing distance becomes shorter than the rated sensing distance, the operation in this kind of environment cannot be recommended.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.