Page top

Primary Contents

Question

Which Ultrasonic Sensors have a long detection distance?

Answer



The E4PA Ultrasonic Displacement Sensor has a long detection distance. Details are provided below.

Long sensing distance suits a variety of applications.

A setting plug with a temperature compensation function makes it easy to set the measurement range.

The Sensor is ultrasonic, so it is not affected by the color of objects.

Perform a variety of control operations by combining with the K3NX Digital Indicator.

Models

Units

Sensing rangeModel
50 to 500 mmE4PA-LS50-M1-N
120 to 2,000 mmE4PA-LS200-M1-N
240 to 4,000 mmE4PA-LS400-M1-N
400 to 6,000 mmE4PA-LS600-M1-N

Accessories (Optional)

Sensor I/O Connectors

CableShapeCable lengthModel
Standard CableStraight
2 m5 conductorsXS2F-D521-DG0-A
5 mXS2F-D521-GG0-A
4-to-5 Conductor Conversion
Cable (See note.)
0.3 m---E4PA-C01

Note:When you use a 4-pole sensor connector cable, the E4PA-C01 is useful for converting from 4 to 5 poles. If this is done, however, you cannot use the mutual interference prevention function.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Ultrasonic Sensors FAQ