![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the withstand pressure of Pressure Sensors?
Answer
Withstand pressure is the pressure that can be withstood for up to 30 s if the rated pressure range is exceeded. For example, the Withstand pressure for E8F2-A01C Pressure Sensor is 400 kPa.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.