![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is linear hysteresis?
Answer
An ideal line is drawn along the output current (or voltage) values for zero pressure and rated pressure to find the amount of error between the actual measured current (or voltage) and the ideal current (or voltage). The linear hysteresis is the maximum absolute value of the difference between the values obtained for pressure rising error and pressure falling error expressed as a percentage of full scale.
Example: The hysteresis for the E8M-10 Pressure Sensor is ±1% F.S.
Converted to voltage,
±1% × 1⁄100 (%) × 4 V (F.S.) = ±0.04 V
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.